PLUS+1 User Forum
PLUS+1 Software => General controls => Topic started by: lijun0 on October 27, 2013, 03:28:54 PM
-
I have a question. How many Plus 1 controller can be connected to the same bus and work properly? 255 ?
Lijun
-
Hi,
I want to try to give an answer:
It depends on the configuration of your system.
Somewhere I have read about 15 IO-Modules?
I have build a system with 2 Can-Joysticks, 1 MC050-10, 1 DP250, 1 IX012 3 OX 024
and the bus traffic was about 60%.
You have to watch the bus traffic.
Controller and Input and Output modules and other modules send every e.g. 20ms information.
You can change this time to a higher parameter if it is OK for your application.
So, look to the traffic!
I hope, this helps a little,
Bernd
-
Hi,
mebib posted a link relevant to this, some time ago.
http://powersolutions.danfoss.com/stellent/groups/publications/documents/product_literature/520l0719.pdf
on page 21, you will find a nice list of estimated CAN-bus loads for the different controllers.
Regards
Jakob
-
Thanks for your reply! I can control the bus load. The concern is hardware that I read from an article which states there is a limit of 110 node on the same bus because of voltage .
best regards
Lijun
-
Interesting, do you have a link to this article?
I doubt that I would ever need above 110 nodes, but never say never. Even silent nodes are nodes too.
But then maybe another bus would be more suitable.