PLUS+1 User Forum

PLUS+1 Software => Displays => Topic started by: macbahi on August 27, 2021, 12:04:23 AM

Title: DP700 BusOn
Post by: macbahi on August 27, 2021, 12:04:23 AM
Hi!!
I had BusOff and the red led blinking.
It was done because the can cable was damaged.
I make new cable but the red led stay blinking.

My question is't possible to make BusOn without restart Display.

Thanks
Mac

Title: Re: DP700 BusOn
Post by: Tor on August 27, 2021, 08:29:10 AM
Hello macbahi,

When the controller goes to BusOff it tries to reset itself a number of times (5 times is default).
This number can be set in the Unit_Config block in the application template. You can also add a manual reset signal, in addition to the existing one. Read the API before before doing this.

If you don't have a manual reset signal you need to restart the unit.

Have a nice day.