PLUS+1 User Forum

PLUS+1 Software => Communication => Topic started by: CPP on April 12, 2013, 08:51:30 PM

Title: CAN Protocols
Post by: CPP on April 12, 2013, 08:51:30 PM
Is it possible to use multiple protocols on one 50pin controller?

ie. CAN_0 - J1939
     CAN_1 - CANOpen
Title: Re: CAN Protocols
Post by: Lammert on April 12, 2013, 11:02:57 PM
Hello,

There is no problem to do that. The both CAN clamps are separate from each other. Only be carefully that you don't use signals from J1939 to CAN_0 and then inside to CAN_1 and then to CANOpen. I had some trouble with.

Regards

Lammert