PLUS+1 Hardware > Controllers
ExecTimeWork ?????
(1/1)
macbahi:
Hi!
I use DM430E I use check point to see ExecTime, ExecTimeGraph and ExecTimeWork but this last I can see it.
Please could you tell if ExecTimeWork is watching. If yes Please show me how can I see it.
thanks in advance
Cordially
mac Bahi
Tor:
Hello mac Bahi,
See attached image, it explains it a little better than I can.
This is taken from the DM1000 API specification, but I believe it works the same for the DM430E.
If you want even more information you can open the DM1x00 API from the hardware tab in PLUS+1 GUIDE (If you have the DM1x00 install that is), and search for "Main and Background Tasks". There are some very useful information.
I hope it helps.
Navigation
[0] Message Index
Go to full version