Author Topic: IO024 CAN Error  (Read 7505 times)

Offline bryantmorris

  • PLUS+1 Expert
  • ****
  • Posts: 51
  • Karma: +0/-1
IO024 CAN Error
« on: July 08, 2016, 07:02:31 AM »
Hello,

I'm working with a SC050-010, a OX024 and 2 IX024 expension modules in a plus+1 program. I'm now getting an error regarding the CAN_Out subpage which I can not access. The error is as below:

The CAN Port on the module is connected, any idea what could be causing this issue?


Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: IO024 CAN Error
« Reply #1 on: July 08, 2016, 08:45:26 AM »
Hi,
Don't use - in the Outputmodule bus name, but use _ instead.

For example, do not write OX024-010, but do write OX024_010.

I had this one too once or twice.
/Jakob