PLUS+1 User Forum
PLUS+1 Hardware => Controllers => Topic started by: FluidPowerTom on April 06, 2023, 08:25:24 PM
-
I've been asked by a larger customer of ours if there's a small controller with little or zero I/O that has two independent CAN bus ports. They need the two CAN ports, but all of their I/O are CAN devices. Is anything in the works that is smaller than a MC024 and has two CAN buses?
-
Hello,
I hope you don't mind that I moved it to the "Controllers" topic instead.
A small controller with minimum I/O and two CAN bus ports.
The only one that I can think of and fits that description is the DM430 with dual CAN. But I guess there's the small question about cost as well.
Have I forgot something? Maybe someone else knows?
Sorry that I didn't have a better answer.
-
Indeed the DM430 actually costs more than the smallest controller with 2 CAN ports (MC024). As you might imagine the cost is really the driving factor, and it seems like I/O - especially outputs - are generally a driving force behind price.
-
Tom out of curiosity what exact model/number MC024 has 2 CAN ports? I thought it only had 1 port.
I know the MC050 has 2 ports.
-
That would be the MC024-130 (11144803) or MC024-132 (11144804)