PLUS+1 Software > Function Library
Automotive Flex
(1/1)
LouisGroen:
Good day guys,
Is there anyone on here that has worked with the Automotive Flex solution supplied by Danfoss?
Thanks
Louis
tomas.vydra:
Hello LouisGroen,
what you want to know?
LouisGroen:
Good day Tomas,
Thanks for replying. I actually have quite a few questions regarding the pin allocations of the application and whether it would be possible to use them for different uses other than those specified by the application? For example, with the Automotive Flex app, they specify the FORWARD & REVERSE signals as Boolean inputs on two of the input pins, but I intend on using the CAN JS1 joysticks to determine these signals, so I want to use these pins for something else completely, like indicator signals or external solenoid activation?
Navigation
[0] Message Index
Go to full version