PLUS+1 Software > Displays
Download time in DM1000
Camox:
Hello,
I work actually on software for DM1000 dysplay.
The download time for add a software in the dysplay in long. During the download the load speed on the dyspaly is 10kb/s.
We can change the load speed ?
Thank in in advance.
Good day
Tor:
Hello Camox,
Yes the download time for the DM1x00 displays are a bit longer than the rest of units. Especially when you are replacing the HWD file and OS.
I recommend to use USB when working with the DM1x00 displays. You will save a lot of time. When it take almost an hour downloading a new OS with CG150, it will only take a minute with the USB.
If you want to order you can find the part number in the image below (11231512). You can also find it in the Data Sheet.
Have a nice day.
Camox:
Hello Thor,
Thank a lot four your response.
I’ll get that cable fast.
Have a nice day
Camox:
Hello Thor,
Is it necessary to have a driver that the cable connection works?
Thanks
Tor:
Hello,
No, the drivers are included in the PLUS+1 Service Tool.
You need to use the Interlink Gateway. See Image.
Have a nice day
Navigation
[0] Message Index
[#] Next page
Go to full version