I have had a failure with our Danfoss PVED-CC S7 valves when the CAN network fails. If the valve was commanded on it keeps going even though the CAN network is down. Is there a parameter that I can set so that if the valve loses the CAN signal it will stop immediately or go to neutral?