Author Topic: which controller to use???  (Read 4555 times)

Offline Diego M

  • PLUS+1 User
  • **
  • Posts: 5
  • Karma: +0/-0
which controller to use???
« on: June 23, 2016, 08:50:59 PM »
Hello everyone,

I need to create an application that requires the controller to store some data to be used in a trending chart later. has anyone done this? which would be the best controller for this purpose.

Thanks

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 95
  • Karma: +2/-0
Re: which controller to use???
« Reply #1 on: June 24, 2016, 02:33:12 PM »
Hi Diego,
It's very much depends on how many points of data you need to store, is it 10 counters for different events, or is it a continuous running log of many values?
Clarifying these questions will help finding an answer to your actual question.

Offline Diego M

  • PLUS+1 User
  • **
  • Posts: 5
  • Karma: +0/-0
Re: which controller to use???
« Reply #2 on: June 24, 2016, 06:03:03 PM »
the controller should be able to log continuously up to 20 variables.
I have used a SC 050 020 controller in the past, if fact I have a spare one that I was hopping I could use.
thanks,

Offline bryantmorris

  • PLUS+1 Expert
  • ****
  • Posts: 51
  • Karma: +0/-1
Re: which controller to use???
« Reply #3 on: August 09, 2016, 03:26:42 AM »
Hello Diego,

Over what time periods did you want to be able to store the logged data of these 20 variables?

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 333
  • Karma: +25/-0
Re: which controller to use???
« Reply #4 on: August 09, 2016, 07:48:10 PM »
You'll want to do the math on how much data you need to store.  That will require understanding the variable size (8-bit, 16-bit, 32-bit...), how often you wish to log these variables, and how long you wish to keep these variables stored before they can be erased.  You've posed the question in a very generic way.  At the very least you need a count of inputs and outputs and signal types before a controller can be recommended.  I'd recommend looking up some of the 'Extended Memory' controllers from the PLUS1 series for any sort of data logging.
« Last Edit: August 09, 2016, 07:51:09 PM by FluidPowerTom »
Mechanical Engineer
Hydra-Power Systems - Distributor - Pacific Northwest