PLUS+1 Software > Telematics

Looking for a sample of Machine Configuration XML file

(1/1)

spittet:
Hi,

I'm now playing with logging and displaying values from a WS503-BP to the portal. From the "WS Remote Solutions Logging Data User Manual", I get that I need to build and edit an XML file for the Machine Configuration. I correctly understand the points listed in this manual but I would prefer to start with a known to be working XML file that I can edit instead of starting from scratch.

Anybody willing to share a sample?

Have a good day!

Sam

FStelzer:
Hello,

attached a demo file.

Regards,
FStelzer

Nilla:
Hi Spittet!

Here is a Danfoss default version of an .xml-file for a WS503. Remember to update the UUID to an individual one otherwise it wont work. A simple UUID generator can be found here https://www.uuidgenerator.net/.

I hope this helps!

Best regards
Nilla
PLUS+1 Helpdesk

spittet:
Hi FStelzer, thanks a lot for the file. I edited it and it's working nicely.

Hi Nilla, the file you posted is the config file for the device itself (should it be a .dod file instead of an .xml?) as i can understand it. I was asking about the xml file for the machine configuration in the portal. Anyway, the one from FStelzer did the trick. Thanks anyway.

Nilla:
Hi spittet!

Sorry I must have included the wrong file in the .ZIP-file, you're right! Here is the correct Danfoss default version of an .XML-file  :)

Best regards
Nilla
PLUS+1 Helpdesk

Navigation

[0] Message Index

Go to full version