Author Topic: UL recognized  (Read 8365 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
UL recognized
« on: October 31, 2015, 02:19:52 AM »
Hello there
I I have looked at the technical information for the controllers and display in order to find out what standards are met.

I was looking for the Short Circuit Current Rating (SCCR) but it only says Sauer Danfoss test, I wonder if any of the controllers and displays are at least UL recognized.

I have compared a Schneider Electric PLC versus a Danfoss controller and The Danfoss are way better and they got more standards met then the SE

I guess they are but not sure, does any body has looked into this?

I got an aplication where the control box should be in compliance with UL 508A, so as far as I understand the standard as long as the device is listed or recognized it can be used.

I appreciate any feedback

thanks