Recent Posts

Pages: 1 [2] 3 4 ... 10
11
Controllers / PWM output, proportional Valve
« Last post by AP on April 17, 2024, 10:40:56 PM »
Hello I am new to Danfoss! THANK YOU FOR ANY HELP!!

I am trying to control a proportional valve with a PWM signal, the valve requires a 0 to 600mA.

What are the steps involve in this. as simple as possible?

1. Scaling. the valve is inversely proportional so 0mA= 3000PSI and 600mA=0PSI, I can use y=mx+b or scale function from library.
2. is there a function block needed to output a PWM? or can I send the scaled value to the Multifunctional Output?
3. how is the ping configuration done? Output mode option 3,4 or 5?

Thank you again !!
12
Displays / Re: DM1000 ver:70312394v330
« Last post by Camox on April 17, 2024, 09:26:55 AM »
I've just tried to update the hardware of a project with a DM1000.
I had a compilation error concerning the RS232 output which I corrected by modifying the data format.

I didn't get any image errors.
Did you get more details about this error?
13
PLUS+1 Autonomy Hardware / Path Follower Block
« Last post by ibrahim on April 17, 2024, 08:52:41 AM »
Hi,

I was trying to create an application that records and follows a path However, I couldn't succeed because the "Path Record" block requires a license.  Can I make the vehicle follow the path by providing an "Example Path" like the attachment "example_path.jpg"?                                                   
* Actually, I have created the following outline for this application (in the attachment-2:Path_Follower_E.jpg). However, the "Path Follower" block does not output "Cmd_Velocity". It only calculates "Cmd_Curvature". I'm not sure if manually setting the "Cmd_Vel" value is the right approach. In this case, I'm not confident if my vehicle is constantly moving to follow the given waypoints. What are your thoughts on this?

Thank you for your support.

Have a nice day
14
Displays / DM1000 ver:70312394v330
« Last post by dlewis on April 16, 2024, 04:24:24 PM »
When trying to update the HWD file in my program I get the following message:

"Replace Missing Image Format"

I've never seen this before when updating a Display HWD file.

What am I supposed to do?

15
PLUS+1 GUIDE / Re: Plus+1 Educational License
« Last post by llang on April 15, 2024, 12:45:30 PM »
You can contact your local danfoss service partner via the "where to buy" button.

https://www.danfoss.com/en/products/dps/software/software-and-tools/plus1-software/#tab-overview

16
PLUS+1 GUIDE / Re: Plus+1 Educational License
« Last post by Salih on April 15, 2024, 08:57:45 AM »
How we get the activation key for educational license?
17
PLUS+1 GUIDE / Re: Plus+1 Educational License
« Last post by llang on April 08, 2024, 08:59:21 AM »
You need to download the danfoss Plus+1 update center. There you can enter your activation key.
18
Function Library / Re: FunctionBlock for Average
« Last post by Lukey on April 04, 2024, 02:27:30 AM »
Try the average filter function block, read up on the user manual this will explain in detail how it works.
19
Function Library / Re: FunctionBlock for Average
« Last post by AP on April 03, 2024, 11:09:12 PM »
Hello, I am new to Plus 1 programming, and need to do a similar task, is there any advice or maybe a screenshot on how to handle it?

Thank you very much!
20
Function Library / Re: PGN RX Not Receiving Data
« Last post by Marbek_Elektronik on April 03, 2024, 09:19:28 AM »
And I think it is doesn't work, if you put 2 RX modules in the program with same ID node.
Pages: 1 [2] 3 4 ... 10