Hello.
I ran into an interesting issue today.
While using the scale function in Guide, if the input is out of the minimum value, or the max value, the output becomes undefined.
Took me a while to figure out what was going on. This is not mentioned in the documentation as far as I can see.
For a solution to this problem I did the following (see attached screenshot)