PLUS+1 Hardware > PLUS+1 Autonomy Hardware
Position Filter in PLUS+1 with XM100
(1/1)
ibrahim:
Hi guys,
I would like to use the Position Filter block in Plus+1. I don't have any issues with the input and output connections. However, when I try to use it, I encounter the following error: 'ERROR 385 (COMPONENT: {O__POU-CALL}. XCLASS: {St_POSITION_FILTER_FB_V300_Ccp} IS UNKNOWN'. Can you provide assistance?"
Navigation
[0] Message Index
Go to full version