Author Topic: DM700 portrait layout or vertical layout  (Read 4269 times)

Offline Beezkneez

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +2/-0
    • Trebro Turf Equipment
DM700 portrait layout or vertical layout
« on: June 08, 2024, 12:31:39 AM »
I am trying to find a setting in the vector based screen editor to flip the display orientation from horizontal to vertical or landscape to portrait. I am not finding it. I searched the manual and still not finding what I am looking for. I’m hoping it’s something simple that I am overlooking. Has anyone done this? Used a screen in a vertical position instead of horizontal or portrait instead of landscape?

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 201
  • Karma: +37/-1
Re: DM700 portrait layout or vertical layout
« Reply #1 on: June 10, 2024, 08:42:39 AM »
In the VBSE Screen Manager panel click on the top level to select it (should be the name of your screen definition). Then in the Inspector panel expand Top Level and you will see rotation.

Offline Link

  • PLUS+1 User
  • **
  • Posts: 9
  • Karma: +0/-0
Re: DM700 portrait layout or vertical layout
« Reply #2 on: June 10, 2024, 08:47:39 AM »
In addition to what Acmall said, in the update center under "Training Video Extras" there is a example project called: "DM1000 Application Example". This example project also has an example of how to switch between Horizontal and Vertical.
« Last Edit: June 10, 2024, 09:11:31 AM by Link »