PLUS+1 Tools > PLUS+1 Service Tool
Download Progress Bar
(1/1)
dlewis:
Has the download progress bar been taken away when downloading programs into controllers? I don't see one anymore.
Tor:
Hello dlewis,
The progress bar in the PLUS+1 Service Tool is still there, at least when I test it in v2022.2.5.
If you still have the issue after a restart of the PC and/or Service Tool please create a case here: https://danfoss.secure.force.com/dpscustomersupport/?Product=service
Have a nice day.
dlewis:
Looks like I'll need to contact tech support. I uninstalled the Service Tool, rebooted the computer and then reinstalled and nothing changed.
dlewis:
I got it !!!
Somehow the portion of the screen that shows the progress bar got pulled all the way to the bottom of the screen. I didn't see it until I FULLY expanded the window. Then I was able to see a glimpse of what I was missing. I was then able to drag that part up to the middle of the screen so that when I resize the window to normal I can see the Progress Bar.
I hope this helps anyone that has the same issue in the future.
Navigation
[0] Message Index
Go to full version