PLUS+1 Hardware > Controllers
MC018 C1p11 error 23 and 665
(1/1)
macbahi:
Hi Guys,
It's my first time I use MC018. I will use all output. Every think it's OK.
All setting output are the same way.
But when I compile the program, I get error only for C1P11.
You find enclosed the pictures of errors
I had update my plus+1 to 2024.1.5.
Thanks in advance
With best regards
Mac bahi
A.Fitz:
It looks like nothing is connected to the DigOut component based on the error.
I would use command "V" to view the connection and verify you have something driving it.
I would bet this is a copy paste error where you forgot to change the name somewhere to correlate to this pin.
macbahi:
Hello Fitz
Thank you very much to answer me.
The error it's was feedback but plus+1 compiler show other thinks.
Since I installed the last version the compilation it's not as before.
Any way thanks sir.
With best regards
mac bahi
Navigation
[0] Message Index
Go to full version