Author Topic: Kvaser Driver Incompatibility  (Read 4611 times)

Offline Scott_MARL

  • PLUS+1 Developer
  • ***
  • Posts: 13
  • Karma: +0/-0
Kvaser Driver Incompatibility
« on: March 18, 2022, 06:25:59 PM »
I noticed that the plus+1 drivers conflict with the Kvaser drives, I am trying to use both the Danfoss CG150 and the Kvaser USBcanII (not at the same time). Only one can have their drivers installed at a time. Has anybody found a work around for using both band of devices on one workstation?
MARL Technologies

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: Kvaser Driver Incompatibility
« Reply #1 on: March 22, 2022, 07:03:01 AM »
Hi Scott_MARL,

I asked around regarding your issue:

"Not something I have seen. I have both Kvaser and PLUS+1 drivers installed and use both CG150 and Kvaser Leaf Pro HS v2 without issues.
Maybe related to the Kvaser USBcanII device.
Please check which Kvaser vs PLUS+1 drivers are used.
What happens when it is not working?"


I only use the CG150 and didn't know there was a conflict.
Is more people seeing this or only Scott_MARL?

Have a nice day.
 
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: Kvaser Driver Incompatibility
« Reply #2 on: March 27, 2022, 01:02:31 AM »
Hi All,

I run both without any issues running service tool 11.1.6 version.
The Kvaser gateway needs to be enabled in the communications gateway options.