Recent Posts

Pages: 1 2 [3] 4 5 ... 10
21
General controls / Re: output of compilation
« Last post by Tor on June 28, 2024, 07:38:17 AM »
Hello federico.furlani

This is connected to a change in PLUS+1 GUIDE 2024.1.3.  See release notes.


Have a nice day.
22
PLUS+1 GUIDE / GUIDE 2024.2.4.6047 Warning on compile?
« Last post by Fredrick on June 27, 2024, 08:15:59 PM »
Hi,

What does this warning mean, and what do I do about it?
See attached .png
23
PLUS+1 CS Hardware / Need help setting up CS10
« Last post by PatrickS on June 27, 2024, 03:33:52 PM »
I'm attempting to setting up a CS10 on one of our applications but couldn't find any real documentation on the whole process.
So far I've connected to the device with my computer via Bluetooth, opened the p1d file and established communication to the CS10 from there.

When I opened the file, it said I have to change the WiFi SSID and password for full access.
I then went to the WiFi page -> Operation tab and see where I believe you change the SSID and password.
However, after I changed those settings and hit 'Save', I just get a message that says 'Operation restricted by gateway. Full access mode is required'.

Not sure what I'm doing wrong, am I suppose to change the SSID and password somewhere else or have I missed a step?
Any help is much appreciated.
24
General controls / output of compilation
« Last post by federico.furlani on June 27, 2024, 12:21:51 PM »
Hi everyone,
which is the differences between a .lhx file and a .p1lhx file?
25
PLUS+1 CS Hardware / Re: CS10 - Remote Service tool
« Last post by Lukey on June 27, 2024, 03:33:21 AM »
We've used both within the last 12 months.

I can say I was thoroughly disappointed in the capabilities/development of the CS10.
To elaborate on that I was hoping/expecting that there would already be a seamless Mobile Service Tool application file that would allow us to use the  Mobile Service Tool to tell the CS10 the wifi credential that it is to connect to, that is not the case, you either have to build that file/api yourself (very difficult) or use GUIDE to configure it, so ultimately it is not end user friendly, only good for the developers.
(In our use case wanted to have a CS10 on a mobile piece of equipment, then the end user would use their mobile device to connect to there wifi, that could be a fixed/known wifi or say their mobile hotspot, but programming it to do so is not a simple, It's not that easy it seems.)

The lag/latency was no different between the two, the thing to remember is that regardless of fiber/wifi or mobile network, the CS device still has to connect to the remote/cloud Danfoss Connect/Service tool server, then redirected to the device, so it is never a direct PC/Machine to CS connection, all traffic goes through the Danfoss server where ever that is.
If lag/latency was a concern I use (installted/on/local to the machine) a PC/Nuk with GUIDE software installed and the CG150 connection at 1mbps, then I would us a RDP/VPN connection to the PC/Nuk to work direct from machine to machine in real time.
26
PLUS+1 CS Hardware / CS10 - Remote Service tool
« Last post by Beezkneez on June 26, 2024, 05:54:34 AM »
Hello,

I was told a long time ago the CS10 was going to eventually be capable of remote service tool connections similar to the CS500. I am unsure if that ever happened but IF it did- I am curious about how many people are using it and what is their take on it? I'd like to know about performance as far as logging lag times go, and also remote download speeds.

I used CS500's in the past and was never impressed with the performance. I have not used them since fall of 2023 so it is possible that has improved some. My hope is that the CS10 remote service tool performs better with the Wi-Fi connection vs. the cellular on the CS500. Hoping someone has some insight on this.

Thank you in advance.
27
Code sharing / Re: Extracting unique identifiers and data from a CAN message.
« Last post by Lukey on June 25, 2024, 06:57:26 AM »
You could write a Structured Text/C Code POU to complete this task
or
In the GUIDE/Page use a mixture of the Array components; Get Array Element or Copy of Array and then use Insert Array Elements to place the values into your new array
28
Code sharing / Extracting unique identifiers and data from a CAN message.
« Last post by BRIan on June 24, 2024, 06:57:41 AM »
I have a CAN message that I want to extract information from:
AA 28 63 14 0 1 73 3
AA 28 61 19 0 1 73 3
AA 28 5F F5 0 1 73 3
AA 28 64 F6 0 1 73 3
AA 28 5F 18 0 1 73 3
AA 28 64 F3 0 1 73 3
AA 28 63 18 0 1 73 3
AA 28 61 15 0 1 73 3
AA 28 5F 22 0 1 73 3
AA 28 64 A2 0 1 73 3
AA 28 5F A4 0 1 73 3
AA 28 64 19 0 1 73 3
AA 28 63 33 0 1 73 3
AA 28 61 25 0 1 73 3
D2 is a unique identifier and D3 is it's value. I want to set up one array with unique identifiers eg 63,61,5F,64 and another array which updates live so the first values from this data would be 14,19,F5,F6 and they would change as new values came in.
Identifiers range from 01 to FF.
Can anyone help? I can't seem to get started.
29
Function Library / Re: DST X5 J1939 Template
« Last post by sanjeewa on June 20, 2024, 07:39:49 PM »
I have used CAN Rx block for Rotary sensor Message Id and it was earlier in the order of execution before the Compliance Block.
After removing the Rx Block, it started working. Problem was that block received the message and the Compliance Block did not receive it.
30
PLUS+1 Service Tool / Canalyser VN1610 instead of Danfoss gateway
« Last post by Thierry_ACE_germany on June 20, 2024, 04:15:38 PM »
Hello ,

For E-steering i only want to use Vector Cananlyser , how can i make it visible in service tool  instead of our Kvaser gateway ?

thanks Thierry
Pages: 1 2 [3] 4 5 ... 10