Author Topic: Not able to download ECU information  (Read 4236 times)

Offline armarbo

  • PLUS+1 Novice
  • *
  • Posts: 1
  • Karma: +0/-0
Not able to download ECU information
« on: September 24, 2021, 05:34:34 PM »
I just started learning this software and I'm not really sure what I'm not doing correctly. I've been following along the youtube tutorial for building the first application and this is where I got stuck. Does this mean that the physical hardware itself has a tool key that I need in order to do anything with it? Any information, or direction, from here would be of great help.
« Last Edit: September 24, 2021, 05:43:30 PM by armarbo »

Offline jashom1

  • PLUS+1 Expert
  • ****
  • Posts: 78
  • Karma: +6/-0
Re: Not able to download ECU information
« Reply #1 on: September 27, 2021, 01:40:59 AM »
Hi,

That's a field used to help in identifying different controllers on the same network.  If you are just using one controller it's not that necessary to use that - Just type in 'undefined' and it will continue.

If you would like a title for your controller it is set in 'Service Tool Data/Application ID in GUIDE.