PLUS+1 Hardware > Controllers

Low current draw

(1/1)

paterianus:
I'm getting faults on two digital outputs on a MC50-20 driving IDEC RJ1S-C-D24 relays.  Am I not drawing enough current to let  the controller know its not an open circuit, if so what is the current needed to fake the system?

brianbassett:
Look at note 5 on the Application Interface Document for the MC050-20.

Basically you need at least 500mA to guarantee that a open load error will not occur.

paterianus:
1/2 amp, is pretty big draw, not to mention the 12watts.

Navigation

[0] Message Index

Go to full version