PLUS+1 Tools > PLUS+1 Service Tool
Service Tool V11.1.5
(1/1)
acmall:
Using Service Tool V11.1.5 to download a program to a display is resulting in a parameter structure changed status message on every download even if the parameter structure has not changed. If I download the same program twice in a row without recompiling the status message shows parameter structure changed and the confirmation dialog displayed.
I have tested a DP610TM, DP570 & DP720 and all display the parameter structure message and confirmation dialog on every download. This only appears to happen with displays as downloading to a MC038-10, MC050-110 & MC088-015 the behaviour is as expected only showing parameter structure changed if the parameters have actually changed.
Is anyone else seeing this behaviour with V11.1.5?
Alastair
Marbek_Elektronik:
Yes, too!
It doesn't apperar in Service-Tool 10.1.7, but in Service-Tool 11.1.5 !
DP700 testet.
Nilla:
Hello everybody!
We are aware of this and are working to solve it. Happens only for Linux based displays.
Best regards
Nilla
PLUS+1 Helpdesk team
Nilla:
Hello everybody!
The issue mentioned here has been solved by the release of v11.1.6 that is available for download using PLUS+1 Update center.
Best regards
Nilla
PLUS+1 Helpdesk team
Navigation
[0] Message Index
Go to full version