PLUS+1 User Forum

PLUS+1 Hardware => PLUS+1 CS Hardware => Topic started by: dlewis on August 11, 2022, 08:26:42 PM

Title: Update CS10 Hdw file
Post by: dlewis on August 11, 2022, 08:26:42 PM
How long should it take to download a new program into a CS10 when going from Hwd version 257 to version 303?  So far it's taking what feels like an eternity.
Title: Re: Update CS10 Hdw file
Post by: FluidPowerTom on December 06, 2022, 07:08:34 PM
I just did it last week, and it took over an hour.  Helpdesk said it was normal
Title: Re: Update CS10 Hdw file
Post by: Tor on December 07, 2022, 11:05:39 AM
Hello,

I'm not an CS expert, so don't quote me on this.

When you change the HWD in a CS product, you also replace the LINUX OS, like in the DM1x00. If you use the CG150 as gateway it will take time. A long time.
You should be able to use WiFi, which is faster (nothing I have done myself, but I heard it takes around 2 minutes).
I'm not sure what happens after the update, if you just can connect with WiFi again or if you need to connect with CG150 and change some settings??
 

Here's a video about the CS10 and WiFi connection: https://youtu.be/fV2DmM28Pro (https://youtu.be/fV2DmM28Pro)

Have a nice day.