PLUS+1 User Forum
PLUS+1 Hardware => Controllers => Topic started by: macbahi on February 01, 2024, 03:28:48 PM
-
Hello all,
I use module SC050, OX024, DM430 and engine
I want to use Can_0 communication only between SC050 and engine.
And use Can_1 communication with SC050, OX024 and DM430.
I think for module OX024 it's ok. It's done Please see image enclosed.
But I don't know if I must to change also Can_0 of DM430 and SC050 secondary to Can_1.
Or just connecting modules to Can_Bus_1.
Specially SC050 secondary.
I hope you understand my idea.
Thanks in advance for you help
With best regards
Mac bahi
-
Hello 8)
SC050:
- For the engine communicatione you need to use CAN0 (CAN port 0)
- For the OX024 and DM430 CAN1 (CAN port 1)
DM430:
- CAN0 (if you are using the physical CAN0)
OX024:
-CAN0
-
Hello mtrbib
thanks
with best regards