Author Topic: Not released for production  (Read 5497 times)

Offline Sergio-DEK

  • PLUS+1 Developer
  • ***
  • Posts: 11
  • Karma: +2/-0
  • Each is a programmer of its own luck.
    • www.dek.si
Not released for production
« on: November 24, 2015, 12:03:18 PM »
Hi!

I'm trying to connect with a MC024-024 controller using the service tool and suitable P1D file.
When I go online and scan the system it responds with status



Does anybody know what it means, or what should I do to connect normally?

Thnx
« Last Edit: November 24, 2015, 12:09:21 PM by Sergio-DEK »
Sergio Kosic
DEK electronics

Offline Loader

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +3/-0
  • If something can go wrong, it will!
Re: Not released for production
« Reply #1 on: November 24, 2015, 01:53:12 PM »
maybe you use a HW file "Beta"!

Offline FStelzer

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +8/-0
Re: Not released for production
« Reply #2 on: November 24, 2015, 02:54:18 PM »
I agree with Loader.

This error Pops up, if there is a HW file on the Controller or better said a "Firmware" which is not released from Danfoss.


KR,
FStelzer

Offline Sergio-DEK

  • PLUS+1 Developer
  • ***
  • Posts: 11
  • Karma: +2/-0
  • Each is a programmer of its own luck.
    • www.dek.si
Re: Not released for production
« Reply #3 on: November 27, 2015, 09:49:58 AM »
Thank you guys for the help. You are right.

I also contacted Danfoss support. They said that the program in the controller is a redesigned "Automotive on PLUS + 1" program made by Gehl/Manitou/Mustang and I'm trying to connect with a standard Danfoss diagnostic file (P1D). Finally I managed to connect and change the necessary parameters.

Regards,
Sergio Kosic
DEK electronics