PLUS+1 User Forum

PLUS+1 Tools => PLUS+1 Service Tool => Topic started by: Sergio-DEK on November 24, 2015, 12:03:18 PM

Title: Not released for production
Post by: Sergio-DEK on November 24, 2015, 12:03:18 PM
Hi!

I'm trying to connect with a MC024-024 controller using the service tool and suitable P1D file.
When I go online and scan the system it responds with status

(https://dl.dropboxusercontent.com/u/4978895/connection_warning.png)

Does anybody know what it means, or what should I do to connect normally?

Thnx
Title: Re: Not released for production
Post by: Loader on November 24, 2015, 01:53:12 PM
maybe you use a HW file "Beta"!
Title: Re: Not released for production
Post by: FStelzer on November 24, 2015, 02:54:18 PM
I agree with Loader.

This error Pops up, if there is a HW file on the Controller or better said a "Firmware" which is not released from Danfoss.


KR,
FStelzer
Title: Re: Not released for production
Post by: Sergio-DEK on November 27, 2015, 09:49:58 AM
Thank you guys for the help. You are right.

I also contacted Danfoss support. They said that the program in the controller is a redesigned "Automotive on PLUS + 1" program made by Gehl/Manitou/Mustang and I'm trying to connect with a standard Danfoss diagnostic file (P1D). Finally I managed to connect and change the necessary parameters.

Regards,