PLUS+1 Hardware > Displays
USB Storage Device not recognized when using CG150-2 and Service Tool ?
(1/1)
Lukey:
USB Storage Device not recognized when using CG150-2 and Service Tool ?
Hardware is DM1x00 Displays, I have tried on both a DM1200T and DM1000T with no success.
Has anyone encountered this?
I am NOT able read/write/see my USB Storage Device connected to the M12, C4—USB Host port when using a CG150-2 and Service Tool
I am able read/write/see my USB Storage Device when using the USB Interlink and Service Tool which is connected on the M12, C3—USB Device port
Navigation
[0] Message Index
Go to full version