Author Topic: new Hex-file for older IO-modules?  (Read 8297 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
new Hex-file for older IO-modules?
« on: July 19, 2012, 03:08:38 PM »
We have a system with 1 Controller and 2 OX024-10.
One Output module is to be changed.
Now, I have an older OX024-10 to use.
The OS ist v140 and the actual version on SD-homepage is v150.
Do you suggest to install the newer firmware to that old module?
The software for the controller would not be changed.
Or is it better not to change firmware ?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: new Hex-file for older IO-modules?
« Reply #1 on: January 20, 2013, 11:52:41 AM »
Ok, I ask again:
Do you prefer to install the newest firmware on older hardware modules such as controllers and IO modules?
Even if you don't need to do this?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

jsaluk

  • Guest
Re: new Hex-file for older IO-modules?
« Reply #2 on: January 31, 2013, 12:12:30 AM »
Upgrade to the latest firmware, old hardware or not.  It apparently cures several issues in the earlier versions.