Author Topic: Service Tool V11.1.5  (Read 7802 times)

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 195
  • Karma: +36/-1
Service Tool V11.1.5
« on: August 28, 2019, 09:05:51 AM »
Using Service Tool V11.1.5 to download a program to a display is resulting in a parameter structure changed status message on every download even if the parameter structure has not changed. If I download the same program twice in a row without recompiling the status message shows parameter structure changed and the confirmation dialog displayed.

I have tested a DP610TM, DP570 & DP720 and all display the parameter structure message and confirmation dialog on every download. This only appears to happen with displays as downloading to a MC038-10, MC050-110 & MC088-015 the behaviour is as expected only showing parameter structure changed if the parameters have actually changed.


Is anyone else seeing this behaviour with V11.1.5?

Alastair


Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 352
  • Karma: +8/-0
    • Marbek Elektronik
Re: Service Tool V11.1.5
« Reply #1 on: August 28, 2019, 10:41:38 AM »
Yes, too!
It doesn't apperar in Service-Tool 10.1.7, but in Service-Tool 11.1.5 !
DP700 testet.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +14/-0
Re: Service Tool V11.1.5
« Reply #2 on: August 30, 2019, 02:02:48 PM »
Hello everybody!

We are aware of this and are working to solve it. Happens only for Linux based displays.

Best regards
Nilla
PLUS+1 Helpdesk team

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +14/-0
Re: Service Tool V11.1.5
« Reply #3 on: November 01, 2019, 11:10:15 AM »
Hello everybody!

The issue mentioned here has been solved by the release of v11.1.6 that is available for download using PLUS+1 Update center.

Best regards
Nilla
PLUS+1 Helpdesk team