Author Topic: DM1000 HWD FILE  (Read 3499 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
DM1000 HWD FILE
« on: October 26, 2019, 03:36:44 PM »
Guys,

has anyone found out the HWD file for the DM1000?   all the technical information is on the web but the 3D model and the HWD, we already have one on order and I need to start working on the firmware

if you have it can you share it?

Thank you

Offline arlemaster

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Re: DM1000 HWD FILE
« Reply #1 on: November 08, 2019, 07:11:03 PM »
There are some HWD for the DM1000 and DM1200, but they are currently not available on the Update Center. Seems like there is still a lot of development being done to them, and so they are selectively giving them out upon request. At this time, the best way to get them is to contact the Plus+1 HelpDesk, and they should be able to share a download link to the files. Then you can install them manually, and start your development work. Hopefully that helps get you going.

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: DM1000 HWD FILE
« Reply #2 on: November 13, 2019, 10:50:11 PM »
you right,

that is what I did, I asked for the HWD to the help center guys

thanks