81
Displays / Applog size and memory usage
« Last post by Lukey on February 29, 2024, 06:35:03 AM »Hello, i am using a DM1200T.
Is there anyway to ready the 32mb applog memory size to determine how much has/is being used?
Reading the OS.RAM and OS.Flash values indicates that the applog memory usage has no influence on these values, as I cannot see an significant changes when writting/reading to the applog memory.
The Write_USB block (designed for the DP720 does not work with this hardware fully) does not give information on Used_Blocks or Free_Blocks unfortunately.
Is there anyway to ready the 32mb applog memory size to determine how much has/is being used?
Reading the OS.RAM and OS.Flash values indicates that the applog memory usage has no influence on these values, as I cannot see an significant changes when writting/reading to the applog memory.
The Write_USB block (designed for the DP720 does not work with this hardware fully) does not give information on Used_Blocks or Free_Blocks unfortunately.