PLUS+1 Software > Function Library

Time Ramp function time units

(1/1)

paterianus:
The function has Inc and Dec loop times but no definition of units, what units are these times in?

Neil:
Hi there

Range - the output will increase (or decrease) by this amount during the Increment time (or Decrement time.)  This basically sets your maximum rate for the change in output.
Decrement time - this is the amount of time in milliseconds it will take for the output to change by the Range amount
Increment time - same, but opposite direction
Neil

Navigation

[0] Message Index

Go to full version