Recent Posts

Pages: 1 ... 3 4 [5] 6 7 ... 10
41
Communication / Re: IFM CR2050
« Last post by Nickyk on December 23, 2021, 10:43:53 AM »
Hello Palle,

Did you make a function block yourself after all?
I'm looking into using a similar I/O module of IFM.

Thanks.
42
PLUS+1™ News / PLUS+1 GUIDE and Service Tool 2021.2 is released
« Last post by Tor on December 23, 2021, 07:22:33 AM »
HO, HO, HO,

PLUS+1 GUIDE and Service Tool 2021.2 is released.
See what's new in the YouTube Video here:  https://youtu.be/QKVV6xa0Hvg

You can get the latest updates in our PLUS+1 Update Center.
What is the Update Center? Get yourself Updated here: https://youtu.be/4n8f8ri-poY


Have a Merry Christmas and a Happy New Year!
43
Displays / Re: DP710 hwd v240 not compatible
« Last post by BrianF on December 20, 2021, 06:50:30 PM »
dlewis,
You must have a brand new display. They changed the LCDs on the displays and the new hardware version supports that change.  I ran into the same problem.  If you read the revision history in the What is New section in version 250. You can get a clue to what changes have been made by Danfoss.

I make a habit to watch which downloads the update center offers.  If one of the hardware files is updated for a module or display that I use, I try to read the revision history file.  It gives me a little bit of a warning that something is about to change.  Sometimes it is just a bug fix and I don't have to do anything, other times I know I need to get a new version of the software ready with the updated hardware file.

I have been caught off guard a few times and had to make emergency builds because a machine went down and we had to replace a module and the replacement was one of the "new and improved" modules. 

44
Displays / DP710 hwd v240 not compatible
« Last post by dlewis on December 20, 2021, 02:14:58 PM »
I just had an issue with a couple of DP710 programs with hardware v240.  After downloading the programs into the displays the display would not show ANYTHING on the screen.  I had this same issue with version prior to 240 but now it's happening again.  If I update the program to hdw rev 250, the issue goes away.
45
Communication / Re: Help how Send many messages
« Last post by acmall on December 20, 2021, 08:55:32 AM »
If you are just getting started with CAN there is a tutorial and some good info here: -
https://www.kvaser.com/about-can/
46
Function Library / Re: J1939 - Fuel Consumption - Reset Trip Info ?
« Last post by Challenger on December 17, 2021, 02:48:20 PM »
I noticed there is a Request Trip reset Block within the DM430 EIC software.

You can find this by opening one of the .p1p files available through the Update Center.
It is in the Main.scs then follow the path below: MAIN!TOP!Output!CAN_Tx!Send_EngineMsgs

It is my understanding you can copy this block out of the EIC software to use in another application.
47
Controllers / Re: file hdw mc024_020
« Last post by tronelec on December 16, 2021, 06:04:32 PM »
tank`s, I'm out in the field and the connection is sporadic, when creating the program with hw mc024_120 and wanting to download the hw mc024_020 service tool gave me a hardware error, but digging I found an old pac file and I was able to install it in plus one guide and migrate the program
48
Communication / Help how Send many messages
« Last post by macbahi on December 16, 2021, 03:09:20 PM »
H! Guys

I am new CAN communication
I am going to send and receive 20 messages. some times I will use J1939.
Please can you tell me about extended option. 
False  11-bit  ID will be from 0 to  0xFFF
True   29-bit  ID will be from 0 to  0xFFFFFFFF.
Is-it correct?  Please could you show documentation and examples
If I choose repetition sending  100ms,  can I use it for all messages.

Thanks in advance
Yours
49
Controllers / Re: file hdw mc024_020
« Last post by Tor on December 14, 2021, 07:33:34 AM »
Hi tronelec,

I'm not sure what the problem is? Do you have more information?

The latest HWD file for the MC024-020 is 10102117v210 and is found in the Update Center.

If you don't have PLUS+1 Update Center installed: https://www.danfoss.com/en/products/dps/software/software-and-tools/plus1-software/#tab-downloads
If you want to know more about PLUS+1 Update Center: https://youtu.be/4n8f8ri-poY


Have a nice day
50
Controllers / file hdw mc024_020
« Last post by tronelec on December 13, 2021, 09:56:33 PM »
please, i need install file from mc024-020
Pages: 1 ... 3 4 [5] 6 7 ... 10