PLUS+1
® GUIDE provides a fixed interface to the hardware through the Hardware Description (also called an HWD). An HWD has the resources, includes all components that can be controlled with a customized application developed in PLUS+1
® GUIDE, that the program needs to compile an application for the selected hardware. A Hardware Description becomes available to the PLUS+1
® GUIDE program by right-clicking the Hardware Description in the Hardware tab to the right when you have GUIDE open.
Documentation for the hardware typically includes a Data Sheet, an API (Application Programming Interface) Specification, and a Template Overview.
Associated with each Hardware Description is a Hardware Template. A Hardware Template simplifies programming by having inputs and outputs that are configured appropriately for the hardware. A Hardware Template becomes available in the application by right-clicking the Hardware Template in the Hardware tab within PLUS+1
® GUIDE.
By the link below all HWD files can be downloaded and installed in PLUS+1
® GUIDE through the Install Hardware options in the Setup menu.;
http://powersolutions.danfoss.com/products/plus-1-software/plus-1-microcontroller--hwd-files/#/ Be sure to read the ReadMe file before you start to use the HWD’s. That can e.g. tell you which version in a package of HWD’s that you should use. The meaning of these acronyms could depend a little bit on where they are used but normally these are the explanations;
For MicroControllers (MC’s)nl = Non-Legacy; a HWD that is used to unleash the full potential of the hardware (e.g. MC0xx-1xx) that supports new symbols, naming conventions etc. and should be your base for future development.
lg = LeGacy; a HWD that supports applications with old-style naming conventions to be able to re-compile MC0XX-0XX applications without changes.
os = Old System; a HWD that supports old CAN and EEPROM symbols.
Normally you should be able to find this information in the Readme-file for each HWD-file.
For DisplaysMoving from a
DP600/610 to a DP600TM/610TM you should use a HWD called DP600/610TM_
os
Moving from a
DP600LX/610LX to a DP600TM/610TM you should use a HWD called DP600/610TM_
lgMoving from a
DP620 to a DP620LX you should use a HWD called DP620LX_
lgAll programmable hardware files (HWD or PAC format) can be used with the Express license in PLUS+1
® GUIDE.
Best regards
Nilla
PLUS+1
® Helpdesk team