Author Topic: Bidirectional PWM drive configuration  (Read 7125 times)

lijun0

  • Guest
Bidirectional PWM drive configuration
« on: December 27, 2013, 04:00:58 AM »
Sir,
I'm to set two port as birdirectional PWM drive. How should I configure and connect the line? For example in MC050-10 use Clp37 and Clp38. I set th Pinconfig=8 in Clp37 and connect the output drive to its outputValue. How should I config in Cpl38? I got compile error.

Lijun

lijun0

  • Guest
Re: Bidirectional PWM drive configuration
« Reply #1 on: December 29, 2013, 04:18:20 AM »
My question is the config in Clp37 is "8", what should be in the Clp38? "0"?

Offline alpinedelta

  • PLUS+1 User
  • **
  • Posts: 5
  • Karma: +1/-0
Re: Bidirectional PWM drive configuration
« Reply #2 on: September 03, 2014, 11:14:20 PM »
Can you tell me what you are trying to drive? A coil? Two coils?

When for example I am driving a 90 series pump EDC bi-directional, I configure two pins with the same PinConfig value. As the EDC has two coils, I connect one side of the first coil to C1p37 and the other to ground. And the other coil, I connect the one side to C1p38 and the other to ground. As far as I know, to have reverse polarity you need to use two pins configured the same way.

Fitzsimmons Hydraulics

  • Guest
Re: Bidirectional PWM drive configuration
« Reply #3 on: October 09, 2014, 09:12:59 PM »
I just did this with an MC024. I made both of my output pinconfigs equal to 8.

Hope this helps.

lijun0

  • Guest
read PPU signal as encoder signal for distance measurement
« Reply #4 on: March 06, 2015, 08:33:11 AM »
Can I use Plus+1 micro. to read PPU signal as encoder signal for distance measurement, at low motor speed?