Author Topic: Screen Editor Preview Bug  (Read 3772 times)

Offline sfl_cntrl

  • PLUS+1 Developer
  • ***
  • Posts: 11
  • Karma: +0/-0
Screen Editor Preview Bug
« on: April 08, 2021, 04:24:47 PM »
I am experiencing a bug in GUIDE in the Screen Editor. When browsing images in the Project Library pane with a Preview window open, the image preview is not cleared when selecting a new image. Image previews are simply placed on top of one another and the images cannot be previewed properly. I have to switch to the Screen Definitions pane to refresh the Preview window for the Project Library pane. An example image of this is attached.

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 191
  • Karma: +36/-1
Re: Screen Editor Preview Bug
« Reply #1 on: April 09, 2021, 09:23:08 AM »
I have not been using Guide V12.2 for reasons mentioned in previous posts but, just checked and I am seeing the same problem here.
V11.1 and V12.1 do not have the problem so appears to be related to V12.2

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: Screen Editor Preview Bug
« Reply #2 on: April 12, 2021, 07:38:41 AM »
Hi,

I just tested this and I have the same problem.
I will report this as a bug.

Thank you for letting us know.
Best regards,
Tor
PLUS+1® SW PAE Team