PLUS+1 Software > Displays
Changing image size in program? vector editor
acmall:
Documentation and tutorials is an area were there is room for improvement. There are some widget tutorials on the Plus+1 YouTube page.
https://www.youtube.com/@PLUS1Software/search?query=widget
Marbek_Elektronik:
Thanks,
i have looked to it.
But also Danfoss could explain better how to work with this special technique.
But compilation time now is about 10 minutes. If I use svg instead of bmp it increases to 16 minutes and I am afraid that widgets increase the compilation time also.
In a few days I will use a new workstation with the fastest processor and 64GB RAM, let me see what will happen ;-)
Lukey:
Yes image/widget do increase compile time, I always try to use .png file type and keep the original file size to the dimensions that I require for the display.
A fast workstation helps yes.
My DM1200T 85mb .p1p take 1min40sec to compile and a very long time to download the 80mb .lhx to the hardware.
Camox:
--- Quote from: Lukey on March 15, 2024, 03:20:41 PM ---My DM1200T 85mb .p1p take 1min40sec to compile and a very long time to download the 80mb .lhx to the hardware.
--- End quote ---
The solution to this problem is in this post : https://www.plus1forum.danfoss.com/index.php?topic=1625.msg5493#msg5493.
Have a nice day
Marbek_Elektronik:
Perhaps using usb port increases the download speed instead of CG150.
I watched this at DP700 and TM610.
Navigation
[0] Message Index
[*] Previous page
Go to full version