PLUS+1 User Forum
PLUS+1 Hardware => Displays => Topic started by: pinias on February 04, 2014, 03:17:43 PM
-
Hello there,
Look I have a MC050-10 controller and 2 DP610 displays connected to the CAN 0 but there is an issue.
When I start up the Service Tool using the CG150 interface cable It scans the system so it sees the controller however for some reason it can not see both displays at the same time
it says: Error, no answer from ECU, see picture attached
So the question is, does any one knows how to fix this?
or what should be change in the firmware so that the service tool can see both displays
I really appreciate any feedback
Regards
Antonio
-
Hi Antonio
You have probably on both displays the same Node ID. All components connected to the same bus need to have a unique Node ID.
Regards
-
I support medib.
You will need to download the program for each display individually making sure that you've set the Node (on the Top Level Page of the program) to a different value for each display.
Sam
-
You will also have to label your signals from each display so that you know which one sent the signal.
I ussually send messages to both displays by ensuring each has a unique node address.
Hope this helps.
BgTwuk
-
got it
yes it Works
thanks