PLUS+1 Hardware > Controllers
Two PVEs on a single OX24-110 pin
(1/1)
Camox:
Hello,
We need to add functionality to a second-hand machine equipped with an OX24-110 module.
The number of outputs available to control a PVE coil is insufficient.
I'd like to know if it's possible to control two PVE coils simultaneously with a single output. Have you ever done this?
Thanks in advance.
Lukey:
PVE Ratiometric coils?
I have not physically tried it but in theory it should work just fine, the output from the expansion module is only a reference voltage to the coil/s, there is no load, there shouldn't be an issue.
Camox:
We use active PVEA.
Thanks
Lukey:
PVEA is Ratiometric yes, therefor I would bet Yes it should work fine with two coils on 1 output.
Regarding Active feedback or passive that shouldn't be a concern as is only related to the Fault Output of the PVE to Input of Controller.
Camox:
Thank you for your answers.
Have a nice day!
Navigation
[0] Message Index
Go to full version