PLUS+1 Software > Function Library

Problem with Widget library

(1/1)

samuelhj:
Hello.

Been a while since I had to program a display, but I'm running into two seperate issues.
Display type: DM430E 0-1-X-X series.
Guide version 2024.4.3

If I add a gauge, adjust parameters, and try to compile I get compiler error.
See attached screenshots.

Another strange issue I noticed, linear gauges do not even fit the display, but since I've never used them, I'm not sure if this is expected behaviour?

Navigation

[0] Message Index

Go to full version