PLUS+1 User Forum
PLUS+1 Hardware => PLUS+1 Compliant Hardware => Topic started by: magitec on March 29, 2023, 05:26:57 PM
-
Hi,
I have a JS1H with 2 buttons, one on the top and one on the shaft (OP present) on the wiring pinout i have on the black connector a Dig out 1 and Dig out 2.
i am feeding 12v to pin 2 (pwr 1) and gnd to pin 1. on the grey connector.
- So do the dig out 1 and 2 output 12v+ when the button is pressed?
- do i also need to add 12v to Pwr 2, Pwr 3 and Pwr 4 too?
[/li]
[/list]
many thanks.
-
It looks like it's a yes on all accounts
-
Perfect thank you. just a few other questions i'm using the PMW output for a 12v reversible output to control a 12v actuator forward is 0 - 12v and then backwards is 12 - 0v which PID file do i require for setting up the limits / proportional control scale.
again thank you, its not something i have used before, i do have the correct CG150-2 cable
-
Hello,
I'm a new danfoss user and I need some help with the below:
Sorry in advance for the below message.
The circuit I'm dealing with in my application include 1 x JS1H single axis PWM joystick, One pump having 2 x 24V proportional solenoid Valves A and B (for Right and Left) rotations respectively, and 1x ON/OFF Solenoid Valve for brake +24 Volts const. I've attached a basic schematic for clarification.
I want to set the joystick parameters to perform the below functions:
- Joystick in Forward: Energizes Solenoid Valve A (Proportionally control its flow) and at the same time energizes brake solenoid Valve with +24V (constant).
- Joystick in Reverse position: Energizes Solenoid Valve B (Proportionally control its flow) pin and at the same time energizes brake solenoid Valve with +24V (constant).
- Joystick in Neutral Position: Solenoid A,B and Brake Solenoid are all de-energized.
Is the above feasible with this joystick? A controller is required?
Thank you very much!