Author Topic: Decompile LHX file / extract LHX from controller  (Read 865 times)

Offline samuelhj

  • PLUS+1 Developer
  • ***
  • Posts: 18
  • Karma: +0/-0
Decompile LHX file / extract LHX from controller
« on: January 15, 2025, 06:59:22 AM »
Hello

Is there any way to decompile an LHX file to get a SCS file out from it? Given that it's not locked with an application key.
And is there a way to extract said LHX from a controller given the same situation?

Best regards,
Samuel

Online Lukey

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +8/-0
Re: Decompile LHX file / extract LHX from controller
« Reply #1 on: January 16, 2025, 01:44:18 AM »
Unfortunately not, if you don't have the original GUIDE program file you're dead in the water.

The LHX file is pure machine code, it can't be reverse engineered or extracted from the controller.