PLUS+1 User Forum
PLUS+1 Software => General controls => Topic started by: CPP on February 10, 2014, 07:07:32 PM
-
Due to space and I?O requirements I am needing to use two MC050-010 modules and some OX modules in the same system. Is there a way to do this or are the two MC's just going to conflict with each other?
-
This is one major selling point of the PLUS+1 ie expandable.
You just need to give each module a unique ID.
-
Also, you may want to keep one MC050 as a "custom" IO unit. I mean, use a MC050 without any bulk/programmable content in it. Only use CAN messages that are directly connected to inputs and outputs of this MC050.
My point is to do not have half a program into a MC050 and the other half into the other MC050 for the sake of easy maintenance and upgrading in the future.
Sam