General Discussion > Off topic
UL recognized
(1/1)
pinias:
Hello there
I I have looked at the technical information for the controllers and display in order to find out what standards are met.
I was looking for the Short Circuit Current Rating (SCCR) but it only says Sauer Danfoss test, I wonder if any of the controllers and displays are at least UL recognized.
I have compared a Schneider Electric PLC versus a Danfoss controller and The Danfoss are way better and they got more standards met then the SE
I guess they are but not sure, does any body has looked into this?
I got an aplication where the control box should be in compliance with UL 508A, so as far as I understand the standard as long as the device is listed or recognized it can be used.
I appreciate any feedback
thanks
Navigation
[0] Message Index
Go to full version