Recent Posts

Pages: [1] 2 3 ... 10
1
PLUS+1 GUIDE / Re: Plus+1 Guide Horizontal&vertical bar modification
« Last post by Lukey on Today at 01:42:45 AM »
It cannot be changed, I've already contacted the help desk about this, apparently it is in the pipeline for development but with no immediate due date.
2
PLUS+1 GUIDE / Plus+1 Guide Horizontal&vertical bar modification
« Last post by macbahi on February 17, 2025, 04:30:13 PM »
Hello,

I installed a new Plus+1 guide version 2024.3.5.  But I didn't like the vertical icon tool bar position?  Please See image enclosed?

Please Could you tell me a way to change the vertical icon tool bar to horizontal?

Thank you very much.

With best regards.

mac bahi
3
Displays / Re: DM1000 ETHERNET
« Last post by Beezkneez on February 06, 2025, 04:12:14 PM »
Hi Tor,

Thanks for the response. I have had an open ticket with helpdesk about this for a few days. Have not heard anything and that is why I posted in the forum.

I am aware of the ethernet output page and how to enable the interface, but how do I use it?

Where do I configure messages or packets to be sent and received and then used within PLUS+1 code? I would like to be able to send/receive data on the ethernet interface and I have not seen anywhere on how to do that with PLUS+1.

What protocols are available on the ethernet interface?

Thanks.
4
Displays / Re: DM1000 ETHERNET
« Last post by Tor on February 06, 2025, 09:09:20 AM »
Hello,

As far as I know Ethernet should work on the DM1000 and some models of the DM700.
What I understand you have to enable it in the template. In the outputs page there is a Ethernet page, and the enable signal needs to be set to True.

If you don't get it to work, please contact PLUS+1 Helpdesk: https://www.danfoss.com/en/products/dps/software/software-and-tools/plus1-software/#tab-support


Have a nice day.
5
Displays / Re: DM1000 ETHERNET
« Last post by Beezkneez on February 05, 2025, 05:02:35 PM »
Any updates on this?

I too would like to use the ethernet interface to communicate with other IP devices. I have not seen anything in documentation on how to achieve this.

Has anyone gotten any info from Danfoss or had any success doing this?
6
PLUS+1 GUIDE / Re: error 65 on CAN open PDO_Rx
« Last post by llang on January 30, 2025, 07:09:54 AM »
Hi Camox,

i'm sorry for the late answer. This was exactly the problem, thanks a lot!
7
Displays / DP200 String variable
« Last post by matibe on January 24, 2025, 10:38:00 PM »
How to attach a string data type to a DP200 display text?
So far, I was able to attach only numerical data types.
8
PLUS+1 GUIDE / Re: error 65 on CAN open PDO_Rx
« Last post by Camox on January 24, 2025, 12:22:31 PM »
Hi, there,
I think it's because you have several identical blocks with the same checkpoint.
You can see on the picture that several blocks have the link symbol.

You can solve this problem by changing the namespace of each identical block so that it is unique:
9
PLUS+1 GUIDE / error 65 on CAN open PDO_Rx
« Last post by llang on January 24, 2025, 09:52:13 AM »
Hey guys,
i'm working on a GUIDE project where i have to receive data from another controller via CANopen.
I've installed the CANopen FB Libary 70264983v101 and used the predefined PDO_Rx function block.



When I compile, *** ERROR 65 *** [GLINK] DOUBLE OUTPUTS, SIGNAL1: {PDO_Rx_CP_Enable}, DIRECTION1: {OUT}, FILE1: {MC88_15T_MC88_1BT.exr}, SIGNAL2: {PDO_Rx_CP_Enable}, DIRECTION2: {OUT}, FILE2: {MC88_15T_MC88_1BT.exr} occurs.

Does anyone have an idea how to fix this? I've attached an image.
Thank you.

10
PLUS+1 GUIDE / Re: ERROR 587
« Last post by Camox on January 21, 2025, 08:35:08 AM »
Hello Tor,
Thank you for your response.
I found a solution by creating a new project and copying the contents of the program in error.

For information, this is a project I've been working on for several weeks and the path is identical.

Have a nice day!
Pages: [1] 2 3 ... 10