PLUS+1 Software > Function Library
SPN Conversion Method - ConvMethDM1 ConvMethDM2
dlewis:
Does anyone know the proper SPN conversion method for a Mercedes 904 engine? I've set the conversion method to 2 but i'm getting a strange 6 digit SPN fault rather than the normal 3 digit fault. I'm using PGN65226 and PGN65227 in my program.
Richard:
Hi,
I had a similar problem (maybe identical even ) with a Deutz engine. Apparently Deutz conversion method was not commonly used in the engine world and as a result a bug in the GUIDE DM block for that specific conversion method was incorrect in the version I was using. I would start by ensuring that your DM blocks are the very latest that Sauer have released.
Good luck
sampler:
Was it possible to find a solution for this Mercedes 904? I struggle with the same problem, i.e. too long and wrong SPNs. The question of how to change the Conv Method? In the DM1_RX library block I don't have the Conv Method input option even though it exists in the block description. I have version DM1_RX 3.00.
pinias:
Just enter into the DM block and edit the conversion method see picture
try 3 or 4
sampler:
In the DM1 block, I do not have the option to choose the type of conversion. In any case, the question is whether the output of the MSG SPN [U32] should send value an SPN code that can be sent directly to the display or the value needs to be processed / decoded somehow?
Another thing is that my ADM2-ECU is sending nothing to the address 0x18FECA so now I see as SPN other errors I currently have come from other J1939 ranges. Does the lack of an FECA address mean that the ADM2-ECU error sending needs to be activated? Bellow list of all ID. ID 105 it is DP600 display.
Navigation
[0] Message Index
[#] Next page
Go to full version