Author Topic: USB Storage Device not recognized when using CG150-2 and Service Tool ?  (Read 2272 times)

Online Lukey

  • PLUS+1 Developer
  • ***
  • Posts: 49
  • Karma: +5/-0
USB Storage Device not recognized when using CG150-2 and Service Tool ?

Hardware is DM1x00 Displays, I have tried on both a DM1200T and DM1000T with no success.

Has anyone encountered this?

I am NOT able read/write/see my USB Storage Device connected to the M12, C4—USB Host port when using a CG150-2 and Service Tool

I am able read/write/see my USB Storage Device when using the USB Interlink and Service Tool which is connected on the M12, C3—USB Device port