Author Topic: Problems with OX024 only PVE outputs working  (Read 7823 times)

Gregor

  • Guest
Problems with OX024 only PVE outputs working
« on: February 17, 2014, 08:19:45 AM »
Hello Everyone,
I have a few problems with some OX024-010 Modules. I´m using a MC050-010 Controller and 5 OX024-010. One on the CAN0 and four on CAN1. They´re running at 500kb/s bus-speed and the busload is around 45-47% wich is alright in my opinion.
The Problem ist only the PVE-Signals ( Pinconfig "6") are working but there were a whole bunch of digital outputs that were inactiv. The Signal way must be se same and i can´t understand where the problem is located

Regards
Gregor

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Problems with OX024 only PVE outputs working
« Reply #1 on: February 17, 2014, 01:12:31 PM »
Do you have the newest software and hardware files?

A long time ago I had had the following problem (Guide V4):
I have driven an output , but the output gives no signal.
The workaround was to put an AND with one side "T" and the other side your signal in front of this output and it had worked!!!

So, please test your outputs by connecting a constant "T" to it. Then you will see, if the hardware is OK.

You can also put checkpoints in front of the output.
And you can look via service tool.
Pleas load all Checkpoints of this pin from service tool and watch them.

Bye
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung