PLUS+1 Hardware > I/O Modules
I/O Modules on the CAN Network
Thomas:
Hi!
Each module will need it's own node number, when they show up in the service tool the node number will be multiplied with 8.
You are using node number 64 / 8 = 8
Please make sure that you do use the latest template to the I/O module you are using, you can find them on our website.
Verify also that the Can_Config settings you have done in the template (inside the master) is matching the parameters inside the I/O module.
Here you can find more information http://www.sauer-danfoss.com/stellent/groups/publications/documents/product_literature/520l0717.pdf
Best regards // Thomas
Federico:
Hola,
Tienes más información aquí, puede ayudarte con la configuración de nodos y direcciones de los módulos de expansión:
http://www.sauer-danfoss.com/stellent/groups/publications/documents/product_literature/520l1029.pdf
Saludos cordiales
You have more information here can help with the configuration of nodes and addresses of the expansion modules:
bgtwuk:
Hi
But does the system not config the Can addressing on system power up by the voltage measured on pin 5?
Bgtwuk
Stefan:
Hello,
Yes, if you are using Address Mode 0.
Best regards
Stefan
Navigation
[0] Message Index
[*] Previous page
Go to full version